Skip to main content

Air conditioning is used for cooling, right? Well, yes, but that is only a small part of the story. 

Modern air conditioning systems are air-to-air heat pumps, which can also be used for heating. But how exactly does that work? And what are the advantages and disadvantages of air conditioning as heating? You can read it in this blog post.

Air conditioning as heating: the story of Julie and David

Julie and David bought a detached house built in the 1960s that they thoroughly renovated. Both the living areas and the bedrooms were originally heated with an electrical system. They replaced it with an energy-efficient and user-friendly air-to-air heat pump from Daikin. David: "The choice for an air-to-air heat pump was quickly made. On the one hand because of the exceptionally low power consumption. On the other hand because of the high level of comfort, such as the fast response time and the possibility to both heat and cool. Our rooms are warm within ten minutes in the winter. In the summer we can cool the rooms down in a few minutes.” To provide the heat pump with electricity, the couple also had solar panels installed on the roof. “Thanks to our solar panels, we have greatly reduced our energy costs for heating and cooling,” they say happily.  

Heating and cooling based on cool air 

The air conditioning systems that allow you to cool and heat are also called heat pumps. They transport heat from one environment to another using a coolant. Innovative air-to-air heat pumps are an environmentally friendly way to extract heat from the air. For example, in the summer you can use the air conditioning to cool the rooms in your house. The heat from inside is then discharged to the outside. In the winter, you reverse the process. The heat pump then extracts heat from the outside air – this is even possible at an outside temperature of -15°C – and then releases that heat to the inside air, in order to heat your home.  

The advantages of heating with air conditioning 

If you decide to buy air conditioning, you may want it to do more than just cool or heat the air. A modern air conditioning system creates a perfect indoor climate. The very best air conditioners even filter the air for unhealthy or irritating particles, such as pollen. Such an integrated system has many advantages: You can connect one outdoor unit to multiple indoor units. You then control each indoor unit separately, for an optimal temperature in each room. The compact heat pumps are easy to install. Even if you only have limited space in your home, it is possible to install one. The advanced inverter and heat pump technologies ensure optimal efficiency and maximum energy savings. You will quickly notice this in your wallet! The air conditioners are available in various models, such as wall or floor models. There is certainly a unit that fits seamlessly with your interior.  

The disadvantages of heating with air conditioning

 If you are renovating, you cannot connect an air-to-air heat pump to existing heat emission systems, such as radiators or underfloor heating. If  you want to keep them, you can combine them with an air-to-water heat pump. Also important: you can connect a maximum of five indoor units to one outdoor unit of an air-to-air heat pump. Do you want to cool and heat more rooms? Then consider a different heat pump system, such as an air-to-water heat pump.  

What does air conditioning with heating cost? 

The price of an air conditioner that can both cool and heat depends on many different factors, such as the number of indoor units, the type of indoor unit, the capacity, the options, etc. For a detailed quote, please contact an installer in your area. Tip: if you are renovating and have a heat pump installed, you may be eligible for a subsidy. 

Our most popular air-to-air heat pumps

Culori disponibile
Set pompă de căldură aer-aer
Culori disponibile
Set pompă de căldură aer-aer
Set pompă de căldură aer-aer

Compară modele (1)

Compară modele

Want to discover the full range of air-to-air heat pumps

Check out our full range and find the model best suiting your needs and interior

More information about air-to-air heat pumps

Find the answers to all the questions you might have about air-to-air heat pumps and how they can work for you

Unitatea interioară a pompei de căldură aer-aer este partea sistemului de pompă de căldură aer-aer amplasată în casă și care furnizează aer condiționat în încăpere.

Selectarea unei unități interioare pentru pompa de căldură aer-aer depinde de nevoile tale specifice, însă este important să înțelegi cum funcționează sistemul ca un întreg. Există tipuri diferite de sisteme de pompă de căldură aer-aer, fiecare având propriile caracteristici unice. Unul dintre cele mai populare tipuri utilizate în case este cel split, care conține două unități: una interioară și una exterioară. În încălzire, unitatea exterioară extrage căldura din aerul exterior și o transferă în interior prin unitatea interioară sau invers atunci când răcește casa.


Există trei tipuri de unități interioare pentru pompa de căldură aer-aer:

Unități de perete

Modelele de perete (Stylish, Ururu Sarara, Daikin Emura, Perfera) vin în diferite dimensiuni și culori pentru a se potrivi cu spațiul tău interior.

Unități de pardoseală

Modelele de pardoseală (Perfera Floor) sunt aparate de aer condiționat de dimensiuni compacte, care se potrivesc perfect sub un pervaz sau într-o cameră în care înălțimea este limitată.

Unități necarcasate, cu montare în tavan

Unități necarcasate cu montare în tavan Dacă nu dorești o unitate interioară vizibilă, poți instala o unitate necarcasată cu montare în pereții falși sau în plafoanele suspendate.

Unitatea interioară a pompei de căldură aer-aer este partea sistemului de pompă de căldură aer-aer amplasată în casă și care furnizează aer condiționat în încăpere.

Selectarea unei unități interioare pentru pompa de căldură aer-aer depinde de nevoile tale specifice, însă este important să înțelegi cum funcționează sistemul ca un întreg. Există tipuri diferite de sisteme de pompă de căldură aer-aer, fiecare având propriile caracteristici unice. Unul dintre cele mai populare tipuri utilizate în case este cel split, care conține două unități: una interioară și una exterioară. În încălzire, unitatea exterioară extrage căldura din aerul exterior și o transferă în interior prin unitatea interioară sau invers atunci când răcește casa.


Există trei tipuri de unități interioare pentru pompa de căldură aer-aer:

Unități de perete

Modelele de perete (Stylish, Ururu Sarara, Daikin Emura, Perfera) vin în diferite dimensiuni și culori pentru a se potrivi cu spațiul tău interior.

Unități de pardoseală

Modelele de pardoseală (Perfera Floor) sunt aparate de aer condiționat de dimensiuni compacte, care se potrivesc perfect sub un pervaz sau într-o cameră în care înălțimea este limitată.

Unități necarcasate, cu montare în tavan

Unități necarcasate cu montare în tavan Dacă nu dorești o unitate interioară vizibilă, poți instala o unitate necarcasată cu montare în pereții falși sau în plafoanele suspendate.

Da, iar dacă îți renovezi proprietatea și treci la un aparat de aer condiționat cu sursă regenerabilă, vei adăuga valoare locuinței renovate, mediului și buzunarului. Pompele de căldură pot fi instalate în orice locuință. Totuși, există câteva aspecte de luat în considerare, mai ales în ceea ce privește izolația. Pentru ca pompa de căldură să funcționeze în modul cel mai eficient, casa trebuie să fie bine izolată pentru a preveni pierderile de căldură. Un inginer calificat în domeniul sistemelor de încălzire îți poate oferi recomandări privind lucrările necesare de efectuat în casă pentru ca aceasta să fie adecvată pentru o pompă de căldură. Poate fi vorba despre modernizarea izolației pereților și a acoperișului. Un alt aspect de luat în considerare este și locația. Unitatea exterioară trebuie instalată în exteriorul locuinței, într-o zonă ușor accesibilă în cazul în care necesită curățare, ajustarea setărilor sau pompa de căldură necesită lucrări de service.

Da, o pompă de căldură aer-aer (cunoscută și ca aparat de aer condiționat) poate produce apă caldă menajeră pentru casa ta. Cu soluția Multi+ de la Daikin, un singur sistem furnizează încălzire, răcire și apă caldă. Acesta se poate conecta la cel mult trei unități și un rezervor de apă caldă menajeră, fiind compatibil cu rezervoare de 90l și 120 l și cu o gamă largă de unități interioare, oferind o flexibilitate de neegalat. Soluția Multi+ include un afișaj în text complet pe rezervorul de apă caldă menajeră pentru monitorizarea și ajustarea tuturor setărilor, inclusiv programare și temperatura apei.

Pompele de căldură aer-aer Daikin pot ameliora alergiile deoarece pot capta alergenii în filtrul pompei de căldură și optimiza calitatea aerului pe care îl respiri. Pompele de căldură aer-aer nu numai că furnizează încălzire și răcire, ci elimină poluanții, polenul și particulele din spațiul în care respiri.

Unele unități Daikin sunt echipate și cu Flash Streamer și diferite filtre precum filtrul din apatit de titan pentru dezodorizare sau filtrul de argint pentru eliminarea alergenilor, care pot reduce rapid și eficient poluanții din aer.

Nu! În plus, pompele de căldură aer-aer (cunoscute și ca aparate de aer condiționat) pot reduce simptomele alergiilor. Daikin integrează în toate unitățile de aer condiționat mai multe filtre: filtre din titan de dezodorizare, filtre de argint împotriva alergenilor și unități Flash Streamer, care elimină praful și captează bacteriile. Aceste filtre vor furniza aer mai curat și mai sănătos pentru respirat dacă acestea sunt curățate periodic și aparatul de aer condiționat este întreținut corespunzător.

Pentru ca pompa de căldură să funcționeze corect, este esențial ca sistemul să fie instalat corect. Instalarea trebuie să aibă loc într-o locație adecvată și să fie executată exclusiv de către un tehnician autorizat. Suprafața trebuie să fie suficient de fermă pentru a suporta greutatea și vibrațiile unității; de asemenea, trebuie să fie suficient spațiu pentru debitul de aer și pentru conectarea conductelor și a cablurilor de alimentare. Orice plante sau arbuști care pot fi situate în apropierea pompei de căldură ar trebui să fie la cel puțin un metru distanță și tăiate în mod regulat. De asemenea, pompa trebuie să fie instalată într-un loc ușor accesibil pentru service și alte lucrări de întreținere generală.

Adesea suntem întrebați de ce nu putem pune pompa de căldură înăuntru. Nu ar putea fi amplasată în pod sau în seră? Răspunsul la aceasta este nu. Acest lucru se datorează faptului că, după câteva ore, pompa de căldură va fi extras toată căldura din aerul captat, transformând efectiv acest spațiu într-un congelator. Acesta este motivul pentru care pompele de căldură aer-aer au nevoie de acces la aerul exterior care circulă liber.

Îți recomandăm să contactezi anual un inginer calificat pentru lucrări de service. Lucrările de service programate, verificările aleatorii din întreținerea periodică și curățarea periodică a sistemului va extinde durata de utilizare a aparatului și va păstra eficiența energetică.

Iată câteva semne care indică faptul că pompa de căldură aer-aer (cunoscut și ca aparat de aer condiționat) necesită întreținere imediată:

Dacă aparatul de aer condiționat face mai mult zgomot decât în mod normal, filtrele pot fi înfundate. Curăță unitatea îndepărtând praful cu un aspirator. Dacă zgomotul persistă sau dacă auzi un sunet de gâlgâit, poate fi o problemă mecanică. Contactează un tehnician calificat pentru a verifica unitatea.

Curious to learn all about air-to-air heat pumps?

Read the full story about air-to-air heat pumps and make an informed decision

Discover more home solutions

At Daikin, we believe that a house becomes a home through comfort, care, and the joy of shared moments. Discover our comfort solutions for your home.