Understanding air-to-air heat pump energy consumption
With energy costs so high, air-to-air heat pump efficiency matters
Energy efficiency is at the forefront of many homeowners’ minds, as they think about protecting the planet and reducing their bills. If you're considering installing an air-to-air heat pump (also known as an air conditioner) to heat and cool your home, it’s sensible to have an idea of how much electricity it will use.
What determines the energy consumption of an air-to-air heat pump?
Many factors affect air-to-air heat pump energy usage and cost to run, including:
- How well insulated your home is and how well it retains warmth or stays cool.
- Its position and orientation. If it's sheltered from the sun and wind, it might need less energy for cooling and heating. If it's south-facing, with lots of windows, it may heat up more in summer (requiring more energy) but be warmer in winter (so need less).
- How large the space is. Bigger spaces take more power to heat and cool.
- How many people live in your home and what their needs are. Babies and elderly people may need a warmer house in winter or struggle more with heat in the summer. It also depends on how much time you spend at home, e.g. if you go out to work.
- If you have blinds or curtains that keep the heat in or block out the sun.
- If you have photovoltaic solar panels to provide “free” electricity.
The type, size and capacity of the air-to-air heat pump units also matters. If they're too small, they won't be effective or efficient. They may have to work harder to heat and cool the room, using more energy, at a higher cost, with less benefit in achieving a comfortable temperature. If they're too big, they'll create excess airflows, which could cause a draught. Again, that's inefficient and costly and may feel unpleasant.
How can I learn more about air-to-air heat pump efficiency and power consumption?
All electric and electronic devices sold in the EU have an energy efficiency rating. These range from A+++ (the most efficient) to D (the least), so you can make an informed choice. You can find the energy labels for all Daikin products on our website.
There are also seasonal efficiency ratings for heating and cooling products that all manufacturers of units sold in the EU must use. The Seasonal Energy Efficiency Ratio (SEER) refers to energy efficiency in cooling, and the Seasonal Coefficient of Performance (SCOP) refers to energy efficiency in heating. They measure efficiency in a typical environment and annual energy consumption.
You can estimate the heat pump energy usage yourself: most manufacturers state the annual consumption of their models in kilowatt-hours on their websites or in their brochures. If you know how much your supplier charges per kilowatt-hour, you can calculate roughly how much your bill will be – bearing in mind the variables above.
Find out more about air-to-air heat pump efficiency in the Daikin product range..
Our most popular air-to-air heat pumps
Compară modele (1)
Compară modele
Culori
Culori
Compare
Want to discover the full range of air-to-air heat pumps
Check out our full range and find the model best suiting your needs and interior
More information about air-to-air heat pumps
Find the answers to all the questions you might have about air-to-air heat pumps and how they can work for you
Unitatea interioară a pompei de căldură aer-aer este partea sistemului de pompă de căldură aer-aer amplasată în casă și care furnizează aer condiționat în încăpere.
Selectarea unei unități interioare pentru pompa de căldură aer-aer depinde de nevoile tale specifice, însă este important să înțelegi cum funcționează sistemul ca un întreg. Există tipuri diferite de sisteme de pompă de căldură aer-aer, fiecare având propriile caracteristici unice. Unul dintre cele mai populare tipuri utilizate în case este cel split, care conține două unități: una interioară și una exterioară. În încălzire, unitatea exterioară extrage căldura din aerul exterior și o transferă în interior prin unitatea interioară sau invers atunci când răcește casa.
Există trei tipuri de unități interioare pentru pompa de căldură aer-aer:
Unități de perete
Modelele de perete (Stylish, Ururu Sarara, Daikin Emura, Perfera) vin în diferite dimensiuni și culori pentru a se potrivi cu spațiul tău interior.
Unități de pardoseală
Modelele de pardoseală (Perfera Floor) sunt aparate de aer condiționat de dimensiuni compacte, care se potrivesc perfect sub un pervaz sau într-o cameră în care înălțimea este limitată.
Unități necarcasate, cu montare în tavan
Unități necarcasate cu montare în tavan Dacă nu dorești o unitate interioară vizibilă, poți instala o unitate necarcasată cu montare în pereții falși sau în plafoanele suspendate.
Unitatea interioară a pompei de căldură aer-aer este partea sistemului de pompă de căldură aer-aer amplasată în casă și care furnizează aer condiționat în încăpere.
Selectarea unei unități interioare pentru pompa de căldură aer-aer depinde de nevoile tale specifice, însă este important să înțelegi cum funcționează sistemul ca un întreg. Există tipuri diferite de sisteme de pompă de căldură aer-aer, fiecare având propriile caracteristici unice. Unul dintre cele mai populare tipuri utilizate în case este cel split, care conține două unități: una interioară și una exterioară. În încălzire, unitatea exterioară extrage căldura din aerul exterior și o transferă în interior prin unitatea interioară sau invers atunci când răcește casa.
Există trei tipuri de unități interioare pentru pompa de căldură aer-aer:
Unități de perete
Modelele de perete (Stylish, Ururu Sarara, Daikin Emura, Perfera) vin în diferite dimensiuni și culori pentru a se potrivi cu spațiul tău interior.
Unități de pardoseală
Modelele de pardoseală (Perfera Floor) sunt aparate de aer condiționat de dimensiuni compacte, care se potrivesc perfect sub un pervaz sau într-o cameră în care înălțimea este limitată.
Unități necarcasate, cu montare în tavan
Unități necarcasate cu montare în tavan Dacă nu dorești o unitate interioară vizibilă, poți instala o unitate necarcasată cu montare în pereții falși sau în plafoanele suspendate.
Da, iar dacă îți renovezi proprietatea și treci la un aparat de aer condiționat cu sursă regenerabilă, vei adăuga valoare locuinței renovate, mediului și buzunarului. Pompele de căldură pot fi instalate în orice locuință. Totuși, există câteva aspecte de luat în considerare, mai ales în ceea ce privește izolația. Pentru ca pompa de căldură să funcționeze în modul cel mai eficient, casa trebuie să fie bine izolată pentru a preveni pierderile de căldură. Un inginer calificat în domeniul sistemelor de încălzire îți poate oferi recomandări privind lucrările necesare de efectuat în casă pentru ca aceasta să fie adecvată pentru o pompă de căldură. Poate fi vorba despre modernizarea izolației pereților și a acoperișului. Un alt aspect de luat în considerare este și locația. Unitatea exterioară trebuie instalată în exteriorul locuinței, într-o zonă ușor accesibilă în cazul în care necesită curățare, ajustarea setărilor sau pompa de căldură necesită lucrări de service.
Da, o pompă de căldură aer-aer (cunoscută și ca aparat de aer condiționat) poate produce apă caldă menajeră pentru casa ta. Cu soluția Multi+ de la Daikin, un singur sistem furnizează încălzire, răcire și apă caldă. Acesta se poate conecta la cel mult trei unități și un rezervor de apă caldă menajeră, fiind compatibil cu rezervoare de 90l și 120 l și cu o gamă largă de unități interioare, oferind o flexibilitate de neegalat. Soluția Multi+ include un afișaj în text complet pe rezervorul de apă caldă menajeră pentru monitorizarea și ajustarea tuturor setărilor, inclusiv programare și temperatura apei.
Pompele de căldură aer-aer Daikin pot ameliora alergiile deoarece pot capta alergenii în filtrul pompei de căldură și optimiza calitatea aerului pe care îl respiri. Pompele de căldură aer-aer nu numai că furnizează încălzire și răcire, ci elimină poluanții, polenul și particulele din spațiul în care respiri.
Unele unități Daikin sunt echipate și cu Flash Streamer și diferite filtre precum filtrul din apatit de titan pentru dezodorizare sau filtrul de argint pentru eliminarea alergenilor, care pot reduce rapid și eficient poluanții din aer.
Nu! În plus, pompele de căldură aer-aer (cunoscute și ca aparate de aer condiționat) pot reduce simptomele alergiilor. Daikin integrează în toate unitățile de aer condiționat mai multe filtre: filtre din titan de dezodorizare, filtre de argint împotriva alergenilor și unități Flash Streamer, care elimină praful și captează bacteriile. Aceste filtre vor furniza aer mai curat și mai sănătos pentru respirat dacă acestea sunt curățate periodic și aparatul de aer condiționat este întreținut corespunzător.
Pentru ca pompa de căldură să funcționeze corect, este esențial ca sistemul să fie instalat corect. Instalarea trebuie să aibă loc într-o locație adecvată și să fie executată exclusiv de către un tehnician autorizat. Suprafața trebuie să fie suficient de fermă pentru a suporta greutatea și vibrațiile unității; de asemenea, trebuie să fie suficient spațiu pentru debitul de aer și pentru conectarea conductelor și a cablurilor de alimentare. Orice plante sau arbuști care pot fi situate în apropierea pompei de căldură ar trebui să fie la cel puțin un metru distanță și tăiate în mod regulat. De asemenea, pompa trebuie să fie instalată într-un loc ușor accesibil pentru service și alte lucrări de întreținere generală.
Adesea suntem întrebați de ce nu putem pune pompa de căldură înăuntru. Nu ar putea fi amplasată în pod sau în seră? Răspunsul la aceasta este nu. Acest lucru se datorează faptului că, după câteva ore, pompa de căldură va fi extras toată căldura din aerul captat, transformând efectiv acest spațiu într-un congelator. Acesta este motivul pentru care pompele de căldură aer-aer au nevoie de acces la aerul exterior care circulă liber.
Îți recomandăm să contactezi anual un inginer calificat pentru lucrări de service. Lucrările de service programate, verificările aleatorii din întreținerea periodică și curățarea periodică a sistemului va extinde durata de utilizare a aparatului și va păstra eficiența energetică.
Iată câteva semne care indică faptul că pompa de căldură aer-aer (cunoscut și ca aparat de aer condiționat) necesită întreținere imediată:
Dacă aparatul de aer condiționat face mai mult zgomot decât în mod normal, filtrele pot fi înfundate. Curăță unitatea îndepărtând praful cu un aspirator. Dacă zgomotul persistă sau dacă auzi un sunet de gâlgâit, poate fi o problemă mecanică. Contactează un tehnician calificat pentru a verifica unitatea.
Curious to learn all about air-to-air heat pumps?
Read the full story about air-to-air heat pumps and make an informed decision
Learn more about air-to-air heat pumps
We've selected some informative and inspirational articles for you to learn more about how Daikin can help you
Discover more home solutions
At Daikin, we believe that a house becomes a home through comfort, care, and the joy of shared moments. Discover our comfort solutions for your home.
Mai multe despre Daikin